Editor Window

The following commands are available in the Kollmorgen Space Editor Window:

Add a new Kollmorgen Space instruction at the end of the current task instructions list.
Add a new user comment line at the end of the current task instructions list.
Assign a label name to the current selected instruction line.
Insert a new Kollmorgen Space instruction or a new user comment into the current selected line.
Edit the current selected line (Kollmorgen Space instruction or user comment). If the line is empty, this command follows the same behavior than pressing the 'Insert' button.
Delete the current selected line (Kollmorgen Space instruction or user comment).

The task tabs allow the user to edit the eight concurrent tasks on the drive handled by the Kollmorgen Space Application Executor on the drive.


  • Task #7 is reserved for emergency handling.

The Application Notes tab allows the user to write comments describing the applications. You cannot program in this tab.

If you right-click inside the Editor Window, the following pop-up menu provides shortcuts for actions: